[iMX8MQ_EVK] on uboot, probing a i2c Device failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[iMX8MQ_EVK] on uboot, probing a i2c Device failed

1,056 Views
jhpark_vine
Contributor III

I added i2c4 device node to  fsl-imx8mq-evk.dts   like below 

&i2c4 {
clock-frequency = <100000>;
pinctrl-names = "default", "gpio";
pinctrl-0 = <&pinctrl_i2c4>;
pinctrl-1 = <&pinctrl_i2c4_gpio>;
scl-gpios = <&gpio5 20 GPIO_ACTIVE_HIGH>;
sda-gpios = <&gpio5 21 GPIO_ACTIVE_HIGH>;
status = "okay";
opt3001@44 {
/* compatible = "ti,opt3001"; */
reg = <0x44>;
};
vl53l1x@52 {
/* compatible = "st,vl53l1x"; */
reg = <0x52>;
};
};

 at uboot promt 

u-boot=> i2c bus
Bus 0: i2c@30a20000
Bus 3: i2c@30a50000  

u-boot=> i2c dev 3
Setting bus to 3

when i probe a i2c device  whose  chip address is  0x44 , it fails . 

u-boot=> i2c probe 0x44
Valid chip addresses:wait_for_sr_state: failed sr=81 cr=a0 state=2020
i2c_init_transfer: failed for chip 0x44 retry=0
wait_for_sr_state: failed sr=81 cr=a0 state=2020
i2c_init_transfer: failed for chip 0x44 retry=1
wait_for_sr_state: failed sr=81 cr=a0 state=2020
i2c_init_transfer: failed for chip 0x44 retry=2
i2c_init_transfer: give up i2c_regs=0x30a50000
 

why probing a i2c device called opt3001  fails?? 

Thanks in advance 

0 Kudos
Reply
1 Reply

1,046 Views
igorpadykov
NXP Employee
NXP Employee

Hi jhpark_vine

 

it may fail due to hadware, so one can check connection to i2c device and check

i2c signals with oscilloscope.

 

Best regards
igor

0 Kudos
Reply