[iMX8MQ EVK] configuring a ecspi device node to fsl-imx8mq.dtsi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[iMX8MQ EVK] configuring a ecspi device node to fsl-imx8mq.dtsi

1,240件の閲覧回数
jhpark_vine
Contributor III

to configure a ecspi node to  fsl-imx8mq.dtsi  , i added  below. 

Actually i, excerpted these  from fsl-imx8mm.dtsi.  

ecspi1: ecspi@30820000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx8mm-ecspi", "fsl,imx51-ecspi";
reg = <0x0 0x30820000 0x0 0x10000>;
interrupts = <GIC_SPI 31 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MM_CLK_ECSPI1_ROOT>,
<&clk IMX8MM_CLK_ECSPI1_ROOT>;
clock-names = "ipg", "per";
dmas = <&sdma1 0 7 1>, <&sdma1 1 7 2>;
dma-names = "rx", "tx";
status = "disabled";
};

 

ecspi2: ecspi@30830000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx8mq-ecspi", "fsl,imx51-ecspi";
reg = <0x0 0x30830000 0x0 0x10000>;
interrupts = <GIC_SPI 32 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_ECSPI2_ROOT>,
<&clk IMX8MQ_CLK_ECSPI2_ROOT>;
clock-names = "ipg", "per";
dmas = <&sdma1 2 7 1>, <&sdma1 3 7 2>;
dma-names = "rx", "tx";
status = "disabled";
};

/*cause  there is no sdma configuration to ecspi3 */ 

ecspi3: ecspi@30840000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx8mq-ecspi", "fsl,imx51-ecspi";
reg = <0x0 0x30840000 0x0 0x10000>;
interrupts = <GIC_SPI 33 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_ECSPI3_ROOT>,
<&clk IMX8MQ_CLK_ECSPI3_ROOT>;
clock-names = "ipg", "per";
/**
dmas = <&sdma1 4 7 1>, <&sdma1 5 7 2>;
dma-names = "rx", "tx";
***/
status = "disabled";
};

Can you check?

Thanks 

 

0 件の賞賛
返信
1 返信

1,231件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信