Hello.
Boot the OS using the W21H2-1-4-1 binary provided by NXP on the iMX8MP reference board.
After startup, the screen will turn off if left without any operation.
After confirming that the screen is off, operate the USB mouse to turn on the screen.
The time it takes for the screen to light up after operating the USB mouse is inconsistent.
(There are times when it is so slow that I feel that the OS is down.)
What is the cause of this?
Do you think it will be improved in future released versions?
I think this phenomenon will become a big problem if we try to release it as a product.
Thanks,
Koji Okuda.