iMX8MP - WebGPU has been disabled via blocklist or the command line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP - WebGPU has been disabled via blocklist or the command line

Jump to solution
1,365 Views
vix
Contributor III

From chromium v117 running on iMX8MP I see the following item in the chrome://gpu page:

  • WebGPU has been disabled via blocklist or the command line.

Disabled Features: webgpu

Is this expected?

I see here some possible reasons, but I don't know which ones apply to the iMX8MP hardware architecture.

Should I pass

--enable-unsafe-webgpu

command line parameter to chromium?

 

Or is this feature unsupported on the iMX8MP hardware?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,332 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
3 Replies
1,351 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Currently WebGPU are not supported by MX8MP in latest BSP, but is pure software.

Regards

0 Kudos
Reply
1,337 Views
vix
Contributor III

Hi @Bio_TICFSL 

do you mean that even with the flags suggested by your colleague here, the implementation is full software?

0 Kudos
Reply
1,333 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

That;s correct!

0 Kudos
Reply