iMX8MP MIPI DSI Bring up:wait payload tx done time out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP MIPI DSI Bring up:wait payload tx done time out

2,464 Views
QiangF
Contributor I

Hi,

We try to bring up MIPI-DSI interface for LCD panel, the panel driver chip is st7701c, we have adapted the code driver by referring to the NXP official tutorial,but also happen the cmd timeout log,like this:

user@imx8mpevk:~$ [   32.946153] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   33.222143] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   33.693853] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   33.953863] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   34.213845] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   34.474231] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   34.737842] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   34.997849] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   35.257562] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   35.517560] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   35.778152] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   36.037555] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   36.297852] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   36.558141] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   36.817553] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   37.077549] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   37.337867] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   37.597543] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   37.857852] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

[   38.117850] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   38.381866] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   38.645573] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   38.906116] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   39.166155] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   39.429539] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   39.689547] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   39.950126] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   40.209539] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   40.470135] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   40.729538] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   40.989870] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   41.249541] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out

[   41.509864] imx_sec_dsim_drv 32e60000.mipi_dsi: wait pkthdr tx done time out

Detailed description is in the attached document

Please give me some guide to fixe this issue

0 Kudos
Reply
2 Replies

2,022 Views
Goran
Contributor I

Hello @QiangF  did you found a solution? I have exactly the same error.

Best regards, Goran

0 Kudos
Reply

2,408 Views
DEEPIKA19
Contributor I

 

Hi @QiangF ,

I would like know if the issue is resolved.

If resolved, could you help me with the solution as I am also facing the same error.

Thanks in advance

Regards

deepika

0 Kudos
Reply