iMX8MP ISI interrupt not firing in de-interlacing mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8MP ISI interrupt not firing in de-interlacing mode

5,195 次查看
mablabs
Contributor I

Hi,

I'm attempting to get de-interlacing using weaving mode working on an iMX8MP. From a previous post, it was suggested to modify the patch on this post (https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ISL79987-and-adv7180-de-interlace-driver...) to support weaving based de-interleaving. It looks like the patch supports weaving based de-interleaving (the iMX8MP application reference manual seems to suggest that only CHNL_IMG_CTRL[DEINT] needs to be set for either odd/even or even/odd de-interlacing, in addition to the rest of the ISI initialization.

However, when I enable odd/even weaving based de-interlacing (by setting deinterlace_mode = <2> in the device tree), it looks like the ISI IRQ is not firing. This is based on looking at the output of /proc/interrupts and observing that the entry for isi is always 0, and that mxc_isi_irq_handler never gets called.

Additionally, when de-interlacing is disabled (by setting deinterlace_mode = <0>), the interrupt does fire (again, by observing that the isi entry of /proc/interrupts increments, and noticing that mxc_isi_irq_handler does get called). 

Do you have any thoughts on what setting could be missing? I have attached the register dump of the ISI of both the weaving based de-interlacing and no de-interlacing.

Thank you for your help.

Mohammed

0 项奖励
回复
7 回复数

5,165 次查看
mablabs
Contributor I

Hi,

I wanted to see if you had an opportunity to look at my post. Are there any registers that I can look at to see why the ISI interrupt is not being triggered?

 

Thanks

0 项奖励
回复

5,143 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you apply all of patches in the community link? but this is for imx8qm, not for imx8mp, and for imx8mp, the capture driver is

"https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx/imx8-mipi-csi2-s..."

0 项奖励
回复

5,130 次查看
mablabs
Contributor I

Hi,

I did apply the patches that were referenced but whenever I enable weaving based de-interlaced mode, the ISI IRQ never gets triggered. Is there something else that I'm missing (from the documentation, it looks like I only need to set the appropriate DEINT value for the CHNL_IMG_CNTRL register). 

I appreciate any help you can provide.

0 项奖励
回复

5,091 次查看
joanxie
NXP TechSupport
NXP TechSupport

I don't know how you apply these patches, but these aren't for imx8mp, refer to the reference manual, you should set CHNL_IMG_CNTRL, did you dump the register?

0 项奖励
回复

5,044 次查看
fatimas
Contributor I

Hi @joanxie 

The register dump is already shared in the earlier post by @mablabs. Just for your reference here is the dump:             

Odd-even:

[ 44.475498] MAB dump_isi_regs -- entry
[ 44.475502] dump_isi_regs -- CHNL_CTRL[0x00]: e0000001
[ 44.475506] dump_isi_regs -- CHNL_IMG_CTRL[0x04]: 20002001
[ 44.475510] dump_isi_regs -- CHNL_OUT_BUF_CTRL[0x08]: 7c707
[ 44.475515] dump_isi_regs -- CHNL_IMG_CFG[0x0c]: f002d0
[ 44.475519] dump_isi_regs -- CHNL_IER[0x10]: 3cfc0000
[ 44.475522] dump_isi_regs -- CHNL_STS[0x14]: 100
[ 44.475527] dump_isi_regs -- CHNL_SCALE_FACTOR[0x18]: 10001000
[ 44.475530] dump_isi_regs -- CHNL_SCALE_OFFSET[0x1c]: 00
[ 44.475534] dump_isi_regs -- CHNL_CROP_ULC[0x20]: 00
[ 44.475538] dump_isi_regs -- CHNL_CROP_LRC[0x24]: 00
[ 44.475541] dump_isi_regs -- CHNL_CSC_COEFF0[0x28]: 00
[ 44.475544] dump_isi_regs -- CHNL_CSC_COEFF1[0x2c]: 00
[ 44.475547] dump_isi_regs -- CHNL_CSC_COEFF2[0x30]: 00
[ 44.475551] dump_isi_regs -- CHNL_CSC_COEFF3[0x34]: 00
[ 44.475554] dump_isi_regs -- CHNL_CSC_COEFF4[0x38]: 00
[ 44.475557] dump_isi_regs -- CHNL_CSC_COEFF5[0x3c]: 00
[ 44.475562] dump_isi_regs -- CHNL_ROI_0_ALPHA[0x40]: 00
[ 44.475569] dump_isi_regs -- CHNL_ROI_0_ULC[0x44]: 00
[ 44.475572] dump_isi_regs -- CHNL_ROI_0_LRC[0x48]: 00
[ 44.475576] dump_isi_regs -- CHNL_ROI_1_ALPHA[0x4c]: 00
[ 44.475579] dump_isi_regs -- CHNL_ROI_1_ULC[0x50]: 00
[ 44.475582] dump_isi_regs -- CHNL_ROI_1_LRC[0x54]: 00
[ 44.475586] dump_isi_regs -- CHNL_ROI_2_ALPHA[0x58]: 00
[ 44.475591] dump_isi_regs -- CHNL_ROI_2_ULC[0x5c]: 00
[ 44.475594] dump_isi_regs -- CHNL_ROI_2_LRC[0x60]: 00
[ 44.475597] dump_isi_regs -- CHNL_ROI_3_ALPHA[0x64]: 00
[ 44.475601] dump_isi_regs -- CHNL_ROI_3_ULC[0x68]: 00
[ 44.475605] dump_isi_regs -- CHNL_ROI_3_LRC[0x6c]: 00
[ 44.475608] dump_isi_regs -- CHNL_OUT_BUF1_ADDR_Y[0x70]: 68700000
[ 44.475613] dump_isi_regs -- CHNL_OUT_BUF1_ADDR_U[0x74]: 00
[ 44.475617] dump_isi_regs -- CHNL_OUT_BUF1_ADDR_V[0x78]: 00
[ 44.475620] dump_isi_regs -- CHNL_OUT_BUF_PITCH[0x7c]: 5a0
[ 44.475625] dump_isi_regs -- CHNL_IN_BUF_ADDR[0x80]: 00
[ 44.475628] dump_isi_regs -- CHNL_IN_BUF_PITCH[0x84]: 00
[ 44.475631] dump_isi_regs -- CHNL_MEM_RD_CTRL[0x88]: 00
[ 44.475635] dump_isi_regs -- CHNL_OUT_BUF2_ADDR_Y[0x8c]: 68400000
[ 44.475638] dump_isi_regs -- CHNL_OUT_BUF2_ADDR_U[0x90]: 00
[ 44.475643] dump_isi_regs -- CHNL_OUT_BUF2_ADDR_V[0x94]: 00
[ 44.475650] dump_isi_regs -- CHNL_SCL_IMG_CFG[0x98]: f002d0
[ 44.475655] dump_isi_regs -- CHNL_FLOW_CTRL[0x9c]: 00
isi interrupt is not generated at all

Thanks

 

0 项奖励
回复

5,004 次查看
joanxie
NXP TechSupport
NXP TechSupport

 I double confirmed internal team that we don’t support Virtual channel mode and we don’t support interlaced mode;

it seems that the RM isn't correct enough,IMX8QM supports virtual channel but imx8mp doesn't

0 项奖励
回复

2,006 次查看
AlexandrP
Contributor III
Hello @joanxie, we have a problem identical to the author of the post. We'd like to use analog cameras in our application, but for effective use we need de-interlacing for analog SD camera support

I looked at the latest publicly available "Processor Application Reference Manual" from August 2024, and it still states that the ISI supports de-interlacing. At the moment we only would like to have weaving method (not blending, doubling, etc), so virtual channel is of no interest

We test using your IMX8MP-EVK board on Linux 5.15 based kernel. Based on the DT bindings I determined that staging drivers were used in `drivers/staging/media/imx/imx8-isi-*`. In it i discovered that in `imx8-isi-hw.c` basic setting for enabling deinterlace was implemented in `mxc_isi_channel_set_deinterlace()`, which was never used in other places

I added it to `mxc_isi_channel_config()` in a similar fashion to `mxc_isi_channel_set_flip()` and tried to initialize `mxc_isi->deinterlace` to 2 and 3. When i set the value to 2 and 3 the isi interrupts stop firing, while when i set it to 0 (de-interlacing disabled) the interrupts work fine

Can you help, how should we approach the issue
0 项奖励
回复