Dear Community,
In order to select a compatible Ethernet PHY for iMX8M Plus, I would like to know what is/are the supported GPIO voltages of the SoC's ENET signals, please ?
I found following info :
From above operational ranges, I would guess that ENET signals could operate with 1.8V mode or 3.3V mode. If this is true, could someone tell me what is necessary configuration to select each mode, please ?
Thanks in advances and best regards,
Khang.
Solved! Go to Solution.
Hi Khang
>From above operational ranges, I would guess that ENET signals could operate with 1.8V mode or 3.3V mode.
right
>NVCC_ENET is a pad/pin of the SoC. So could you confirm that by tying it to 1V8 or 3V3 will allows
>to select the corresponding mode ?
yes correct. For example of connections one can look at i.MX8M Plus EVK schematic
Best regards
igor
Hi again,
I found that NVCC_ENET is a pad/pin of the SoC. So could you confirm that by tying it to 1V8 or 3V3 will allows to select the corresponding mode ?
Best Regards,
K.
Hi Khang
>From above operational ranges, I would guess that ENET signals could operate with 1.8V mode or 3.3V mode.
right
>NVCC_ENET is a pad/pin of the SoC. So could you confirm that by tying it to 1V8 or 3V3 will allows
>to select the corresponding mode ?
yes correct. For example of connections one can look at i.MX8M Plus EVK schematic
Best regards
igor
Thanks @igorpadykov for the confirmation.
Best Regards,
K.