Hi Community,
After successful DDR training for our custom board, I am now facing with new problem :
U-Boot SPL 2021.04-lf_v2021.04+gd1528947bd (Sep 06 2021 - 08:48:23 +0000)
pca9450_bind: 'pca9450@25' - found regulators subnode
pmic_bind_children for 'pca9450@25' at node offset: 5064
Bound: 0 children for PMIC: 'pca9450@25'
pca9450_bind: pca9450@25 - no child found
pmic_reg_write: reg=c, value=29 priv->trans_len:1, ret=0
pmic_reg_write: reg=10, value=59 priv->trans_len:1, ret=0
pmic_reg_write: reg=1e, value=18 priv->trans_len:1, ret=0
pmic_reg_write: reg=8, value=a1 priv->trans_len:1, ret=0
DDRINFO: start DRAM init
DDRINFO: cfg clk
DDRINFO: DRAM rate 3200MTS
DDRINFO: ddrc config start
DDRINFO: ddrc config done
DDRINFO:ddrphy config start
DRAM PHY training for 3200MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000002]
[PMU Major message = 0x00000001]
[PMU Major message = 0x0000000a]
[PMU Major message = 0x000000fd]
[PMU Major message = 0x000000fe]
[PMU Major message = 0x00000004]
[PMU Major message = 0x00000003]
[PMU Major message = 0x00000009]
[PMU Major message = 0x00000007]
Training PASS
DRAM PHY training for 3200MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000006]
[PMU Major message = 0x00000005]
[PMU Major message = 0x00000007]
Training PASS
DDRINFO: ddrphy config done
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
WDT: Not found!
Trying to boot from BOOTROM
image offset 0x8000, pagesize 0x200, ivt offset 0x0
Can't support legacy image
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
Compared to a running image on EVK, it looks like that BL31 image is not found :
U-Boot SPL 2021.04-lf_v2021.04+g1c0116f3da (Sep 06 2021 - 08:48:23 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 4000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
WDT: Not found!
Trying to boot from BOOTROM
image offset 0x8000, pagesize 0x200, ivt offset 0x0
NOTICE: BL31: v2.4(release):lf-5.10.52-2.1.0-rc1-39-gbb4957067
NOTICE: BL31: Built : 04:45:39, Sep 8 2021
U-Boot 2021.04-lf_v2021.04+g1c0116f3da (Sep 06 2021 - 08:48:23 +0000)
CPU: i.MX8MP[8] rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 30C
Reset cause: POR
Model: NXP i.MX8MPlus LPDDR4 EVK board
DRAM: 6 GiB
Knowing that there's no eMMC but only micro SD card available in our custom design, similar to the 8MPLUSDR4-CPU design.
Could you help to guide us to go further, please ?
Thanks in advance and best regards,
Khang