iMX8MN Power-On Sequence issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8MN Power-On Sequence issue

跳至解决方案
770 次查看
justin_hsieh
Contributor II

Hi Team,

Regarding the iMX8MN specifications, only typical and maximum values are provided, but there is no minimum value given.

justin_hsieh_3-1736301936490.png

justin_hsieh_2-1736301882596.png

Our PA team believes that a minimum value should be a positive number even if not specified in the specifications.

The measurement result in our device is -9.54ms, and we have verified the timing on the iMX8MNANOD3L EVK, obtaining a similar value.

Can we bypass this issue?

 

Our device

justin_hsieh_1-1736301839692.png

iMX8MNANOD3L EVK

justin_hsieh_0-1736301800254.png

Please advise.

0 项奖励
回复
1 解答
704 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The minimum value for T3 is not defined means 32K_RTC_XTALI can be earlier than RTC_RESET_B. The test result is just fine.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
705 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The minimum value for T3 is not defined means 32K_RTC_XTALI can be earlier than RTC_RESET_B. The test result is just fine.

0 项奖励
回复
724 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I am help confirm it, when I finshed it I will share to you as soon as possible.

0 项奖励
回复