iMX8MN FlexSPI for ADC input

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8MN FlexSPI for ADC input

跳至解决方案
1,698 次查看
evancornell
Contributor III

Can iMX8MN (specifically MIMX8MN5DVPIZAA i.MX 8M Nano UltraLite Quad) FlexSPI peripheral be used to acquire data from LTC2315-12 high speed ADC? The eCSPI seems to have a maximum read clock frequency of 1/43ns = 23.2 MHz, which isn't enough to clock out the data from ADC. But FlexSPI can do 66 MHz, which should be fast enough. 

Also, can FlexSPI be made to have synchronous clock with SAI audio module? I need to run SAI at fs = 768 kHz (4 data lines, 8 channels), so SAI_MCLK ought to run at 49.152 MHz (768 kHz * 64 bits), and I'd like the FlexSPI to run at a related clock frequency to SAI peripheral.

Thanks!

0 项奖励
回复
1 解答
1,667 次查看
evancornell
Contributor III

Hello, wondering if anyone at NXP can help with the above question.. thanks!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,668 次查看
evancornell
Contributor III

Hello, wondering if anyone at NXP can help with the above question.. thanks!

0 项奖励
回复
1,666 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @evancornell,

Please accept my apologies for the delayed reply.

For the first question the FlexSPI interface for iMX8M Mini can achieve 66MHz is enough to collect the ADC data. However, I'm not sure if your ADC LTC2315-12 has an appropriate SPI interface.

"The LT2315-12 communicates with microcontrollers, DSPs, and other external circuitry via a 3-wire interface. A falling CS edge starts a conversion and frames the serial data transfer. SCK provides the conversion clock for the current sample and controls the data readout on the SDO pin of the previous sample."

You can try interfacing this ADC with the iMX setting up registers for the timing requirements of your ADC.

Regarding the second question, you will need to analyze the clock tree on iMX8M Mini Reference Manual section 5.1.3 Clock Tree and then configure the PLL using this manual.

If you have any questions or concerns, don’t hesitate to let me know.

Have a great day.

Best regards, Brian.

0 项奖励
回复