Can iMX8MN (specifically MIMX8MN5DVPIZAA i.MX 8M Nano UltraLite Quad) FlexSPI peripheral be used to acquire data from LTC2315-12 high speed ADC? The eCSPI seems to have a maximum read clock frequency of 1/43ns = 23.2 MHz, which isn't enough to clock out the data from ADC. But FlexSPI can do 66 MHz, which should be fast enough.
Also, can FlexSPI be made to have synchronous clock with SAI audio module? I need to run SAI at fs = 768 kHz (4 data lines, 8 channels), so SAI_MCLK ought to run at 49.152 MHz (768 kHz * 64 bits), and I'd like the FlexSPI to run at a related clock frequency to SAI peripheral.
Thanks!