iMX8MM: MIPI DSI commands before enabling the CLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MM: MIPI DSI commands before enabling the CLK

10,856 Views
pierluigi_p
Contributor V

Hi All,

a custom display manufacture requires receiving init commands before activating the clock.

If I try sending the commands during the panel_prepare function, I get the following kernel errors

   imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
   panel-simple-dsi 32e10000.mipi_dsi.0: Failed to send DCS (-16), (1)01
   imx_sec_dsim_drv 32e10000.mipi_dsi: panel prepare failed: -16

Is there any way to overcome the problem?

Thanks

Regards

Pier

20 Replies

9,977 Views
StanislavR
Contributor I

We are working on similar project with i.MX8M Mini and have similar results as oferausterlitz.

"If the commands are sent from the enable function (as for most of the MIPI displays drivers), the commands are sent correctly, but the display shows nothing.

If the commands are sent from the prepare function (not seen in other MIPI displays drivers), we get the errors reported in the 1st message of this thread."

 

Do you have any progress in solution of this issue?

0 Kudos
Reply

5,103 Views
ajita02
Contributor IV

Hi StanislavR ,

I have facing same issue with MIPI-DSI panel. can you please provide a lead? I have been stuck on this.

Thanks,

Ajita

0 Kudos
Reply

10,145 Views
nxp31
Contributor II

Regarding your question:

> kernel errors

> imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
> panel-simple-dsi 32e10000.mipi_dsi.0: Failed to send DCS (-16), (1)01
> imx_sec_dsim_drv 32e10000.mipi_dsi: panel prepare failed: -16

I added a new display (the ORIC ORC03003N-40) using the Sitronix ST7701 driver chip  to the iMX8MM EVK.

I patched the Raydium rm67191 driver by only changing the init sequence to the manufacturer command set of the new display, adjusted the pixel clock, and corrected the number of lanes in the corresponding dts and I immediately got colored stripes shown on the display.

One important observation is that the raydium driver uses

mipi_dsi_generic_write() to send mipi commands, which is working, while mipi_dsi_dcs_write_buffer() failed with "wait payload tx done time out" or ""wait pkthdr tx done time out" errors (in kernel log) after about four successful writes.

Find patches for i.MX8MM Android 10 sources below.

Apply with

cd imx-android-10/android_build/vendor/nxp-opensource/kernel_imx

git apply 0001-add-st7701-driver-shows-stripes-not-finished.patch

cd imx-android-10/android_build/device/fsl

git apply 0001-change-mipi-display-to-st7701.patch

0 Kudos
Reply

9,895 Views
electronic15
Contributor III

Hi nxp31, 

I'm also writing a driver for a MIPI panel and I have a doubt about the "mipi_dsi_generic_write()" function. When I send a MIPI command using this function, does it add the PacketHeader and the checksum to the message? Should I send just the payload of the message?

Supouse I have to send 

PacketHeader[39 04 00 XX]
Payload[ B9 FF 83 94 ]
CheckSum [XX XX]

Would it be something like this....?

struct mipi_dsi_device *dsi;

uint8_t mymessage[] = {0xB9, 0xFF, 0x83, 0x94};

mipi_dsi_generic_write(dsi , (void*) mymessage, 4 ); // is this how it works?

....

 

Best Regards!

0 Kudos
Reply

9,887 Views
Yuri
NXP Employee
NXP Employee

@electronic15 
Hello,

   Please create separate request

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

Regards,
Yuri.

0 Kudos
Reply

10,145 Views
pierluigi_p
Contributor V

Hi Yuri,

thanks for pointing this out.

Can you please clarify if both of the bits (1 & 3) must be set?

The current sec-dsim driver, in LP mode currently enables only bit 7 (ESCMODE_CMDLPDT): is this required too?

Thanks

Best Regards

Pier

0 Kudos
Reply

10,145 Views
Yuri
NXP Employee
NXP Employee

Hello,

it depends on customer's requirement, both clock lane and data lanes have the low power state.

Regards,

Yuri.

0 Kudos
Reply

10,145 Views
Yuri
NXP Employee
NXP Employee

Hello,

  To set LP11 mode before initialize the panel, it is possible to set register DSI_ESCMODE:

Bit 1: TxUlpsClk: Specifies ULPS request for clock lane.

Bit 3: TxUlpsDat: Specifies ULPS request for data lane.

Regards,

Yuri.

0 Kudos
Reply

10,145 Views
oferausterlitz
Senior Contributor II

Hi Rogerio,

I attached the datasheet here:

   https://support.nxp.com/s/case/5002p00002FrFGv 

The feeling is that the display controller is not able to accept LPM commands once the MIPI interface switched to HS.

The EVK from the manufacturer shows that all the commands are sent before the MIPI CLK switch to HS.

From a linux kernel perspective, this means that the commands should be sent from the "prepare" function of drm_panel_funcs struct, called before the "enable" function of drm_panel_funcs struct.

If the commands are sent from the enable function (as for most of the MIPI displays drivers), the commands are sent correctly, but the display shows nothing.

If the commands are sent from the prepare function (not seen in other MIPI displays drivers), we get the errors reported in the 1st message of this thread.

Please let me know if you need further details.

Thanks

BR

Pier

0 Kudos
Reply

4,186 Views
Udhay_
Contributor III

hi @oferausterlitz 

can you please tell me according to commands if i movie init sequence prepare function to enable function display is not able to on.what are the possibilities to on the display? i have bought this display from orient display and i am stuck on this.. in your case it worked?

0 Kudos
Reply

9,972 Views
StanislavR
Contributor I

We are working on similar project with i.MX8M Mini and have similar results as oferausterlitz.

"If the commands are sent from the enable function (as for most of the MIPI displays drivers), the commands are sent correctly, but the display shows nothing.

If the commands are sent from the prepare function (not seen in other MIPI displays drivers), we get the errors reported in the 1st message of this thread."

 

Do you have any progress in solution of this issue?

0 Kudos
Reply

9,917 Views
Yuri
NXP Employee
NXP Employee

@StanislavR 
Hello,

   Please create separate thread, if You have an issue.

  

Regards,
Yuri.

0 Kudos
Reply

10,145 Views
rogerio_silva
NXP Employee
NXP Employee

Hi Ofer,

I'll check if it's possible to enter in LPM after switch to HS Mode.

I can't download the datasheet. Could you please send me by e-mail? rogerio.silva@nxp.com

Thanks,

Rogerio

10,144 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I attached the Datasheet to internal thread.

Regards,

Yuri.

10,145 Views
rogerio_silva
NXP Employee
NXP Employee

Thanks Yuri!

Rogerio

0 Kudos
Reply

10,145 Views
rogerio_silva
NXP Employee
NXP Employee

Hi Pierluigi, Andreas,

I'm not understanding what exactly waveform is expected by display. Could you please send the display datasheet?

Best regard,

Rogerio

0 Kudos
Reply

10,145 Views
kislingera
Contributor I

Hello,

I just made some new measurements with the working Board (which uses a SSD2828 bridge; and no iMX).

I assume that the following transmission is a standard LowPower transmission, which every MIPI device should support - and therefore also the iMX8M mini, right?

Clock should be restored by Exor-function of D0P / D0N - right? --> the measurement shows something like 7.4MHz clock frequency for this transmission.

Packet01_CLKP_DISPRST_D0P_D0N__10us_1.png

0 Kudos
Reply

10,145 Views
pierluigi_p
Contributor V

Hi Yuri,

we are currently based on kernel 4.14.98 v2.0.0.

I've also inspected and back-ported the additional sec-dsim patches from kernel 4.14.98 v2.3.0, but the behavior is exactly the same.

Any suggestion?

Thanks

Best Regards

Pier

0 Kudos
Reply

10,145 Views
kislingera
Contributor I

Working on the same project, I can show this picture with another evalboard driving the discussed display. But as Pier wrote above, we need it with MIPI from imx8m mini.

Here you can see the initial code, without having signals on CLK_P (I have also measured CLK_N, but not visible here)

Please excuse the bad signal quality, but I only have one active probe.

URT_PowerUp_20200121.jpg

0 Kudos
Reply

10,145 Views
Yuri
NXP Employee
NXP Employee

Hello,

  What NXP Linux BSP is used in the case?

Regards,

Yuri.

0 Kudos
Reply