I know the newer EVKs have switched to the AzureWave wifi modules.
Is it possible to still get an older EVK with the Murata qca9377 wifi module working with Yocto linux L5.10.35
If so how?
I do not know which version these patches were made for but they do not take for kernel 5.10
So I tried to manually apply the modifications using the patch file as a reference and while I could get it compile the run time crashed.
I checked that nxp doesn't support QCA9377 since 5.4.47 bsp, if customer needs porting this on the newer bsp, pls refer to the 5.4.24 bsp as reference
you can refer to the link as below:
"https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-of-QCA9377-in-Linux5-10-9/ta-p/126..."