iMX8MM-EVK LPDDR4 not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MM-EVK LPDDR4 not work

1,355 Views
kieuvietdich
Contributor II

Hi guys,

I'm used sample iMX8MM-EVK pcb from NXP to make a board, 100% like iMX8MM-EVK.

When I using MSCALE_DDR_TOOL version 310 to test LPDDR4. Calibration and street test OK. Result is attached bellow.

But, when I try to read or write ddr address (like : 0x2000000),  MSCALE_DDR_TOOL alert me that MCU will be hungup. I can load imx-boot-imx8mmevk-sd.bin-flash_evk and run u-boot SPL. When I try to read or write ddram from u-boot, MCU hangup and reseting. 

Can you tell me why? and how to fix it?

Thank you and br,

This my log,

Downloading file 'bin\lpddr4_train1d_string.bin' ..Done

Downloading file 'bin\lpddr4_train2d_string.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_1d_imem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_1d_dmem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_2d_imem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_2d_dmem.bin' ..Done

Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done

Download is complete
Waiting for the target board boot...

===================hardware_init=====================

********Found PMIC BD718XX**********
hardware_init exit

*************************************************************************

*************************************************************************

*************************************************************************
MX8 DDR Stress Test V3.10
Built on Feb 5 2020 13:04:09
*************************************************************************

--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x93d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 1500MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 2048MB
Total density detected on the board is: 2048MB
============================================

MX8M-mini: Cortex-A53 is found

*************************************************************************

============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1500Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @200Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @50Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 2D-Training @1500Mhz...
[Process] End of initialization
[Process] End of 2D read delay/voltage center optimization
[Process] End of 2D read delay/voltage center optimization
[Process] End of 2D write delay/voltage center optimization
[Process] End of 2D write delay/voltage center optimization
[Result] PASS

============ Step 2: DDR memory accessing... ============
Verifying DDR frequency point0@1500MHz.......Pass
Verifying DDR frequency point1@200MHz.......Pass
Verifying DDR frequency point2@50MHz.......Pass
[Result] OK

============ Step 3: DDR parameters processing... ============
[Result] Done

Success: DDR Calibration completed!!!
DDR Stress Test Iteration 1
--------------------------------
--Running DDR test on region 1--
--------------------------------

t0.1: data is addr test
....
t0.2: row hop read test
...

t1: memcpy SSN armv8_x32 test
....
t2: byte-wise SSN armv8_x32 test
..
t3: memcpy pseudo random pattern test
....................................................................
t4: IRAM_to_DDRv1 test
...

t5: IRAM_to_DDRv2 test
--------------------------------
--Running DDR test on frequency point1@200MHz--
--------------------------------

t0.1: data is addr test
....
t0.2: row hop read test
...

t1: memcpy SSN armv8_x32 test
....
t2: byte-wise SSN armv8_x32 test
..
t3: memcpy pseudo random pattern test
....................................................................
t4: IRAM_to_DDRv1 test
...

t5: IRAM_to_DDRv2 test
--------------------------------
--Running DDR test on frequency point2@50MHz--
--------------------------------

t0.1: data is addr test
....
t0.2: row hop read test
...

t1: memcpy SSN armv8_x32 test
....
t2: byte-wise SSN armv8_x32 test
..
t3: memcpy pseudo random pattern test
....................................................................
t4: IRAM_to_DDRv1 test
...

t5: IRAM_to_DDRv2 test

Success: DDR Stress test completed!!!

Labels (1)
4 Replies

1,207 Views
kieuvietdich
Contributor II

Hi igorpadykov,

Thanks for your reply. In two months ago, we make an other PCB for check, but it's same result. 

Yes, you right. 0x2000000 is invalid address. My LPDDR4 seem be worked. I still can't boot use SDCARD or eMMC or QSPI.

When I run Linux over USB downloader UUU, it's worked. But when I set bootmode for automatic boot from sdcard or eMMC or QSPI, my custom board not work. Console not print anything.

Can you tell me how to check bootmode by bare-metal application run on iMX8M-Mini? Or anything I can do to check my custom board. Step by step bringup custom board, etc.

Thanks you.

0 Kudos

1,209 Views
Danube
Contributor IV

Hi

If uuu can work , you can try to show 0x30390058 (SRC_SBMR1) and 0x30390070  (SRC_SBMR2) in debug port.

You can know your Boot_Config is correct or not.

pastedImage_1.png

pastedImage_2.png

1,209 Views
kieuvietdich
Contributor II

Thanks you, my bootmode wrong. It's can boot from flexQSPI now.

0 Kudos

1,209 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kieu

valid ddr memory addresses are described in sect.2.1.2 Cortex-A53 Memory Map

i.MX 8M Mini Applications Processor Reference Manual

seems 0x2000000 is not valid address. Also it is necessary to pay attention

to Chapter 4 How to bring up a new MX8MSCALE board MSCALE_DDR_Tool_User_Guide.pdf

included in ddr test package for performing necessary uboot changes.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos