Hi,
I am working with iMX8MM EVK board. On checking the schematics of the board EXP_CN
UART3_TXD PAD ALT5 function is GPIO_27
UART3_RXD PAD ALT5 function is GPIO_26
I believe we can use them GPIOs in iMX8MM EVK system, adding the below pin control mux
pinctrl_gpiopin3: gpiopin3 {
fsl,pins = <
MX8MM_IOMUXC_UART3_RXD_GPIO5_IO26 0x14f
>;
};
pinctrl_gpiopin2: gpiopin2 {
fsl,pins = <
MX8MM_IOMUXC_UART3_TXD_GPIO5_IO27 0x19
>;
};
Please let me is my understanding is correct and anything more to add.
Thank you,
Sreedhar
Hi Sreedhar
yes your understanding is correct.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you igor !!
Hello,
I have some questions.
Why 0x19 and 0x14f?
When I change the dtsi file and run bitbake, it will update the image with my new dtsi file?
Regards.