iMX8M: virtual channel support in CSI-2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M: virtual channel support in CSI-2?

4,908 Views
ensc
Contributor III

Hello,

iMX8M reference manual says in 13.6.1.1 that the MIPI-CSI2 controller supports virtual channels?  How can I configure them?  E.g.:

- how can I filter out data of virtual channel 2?

- is it possible to implement HDR with iMX8M?  Lines are interleaved in difference virtual channels; how can they be recombined?

Tags (1)
6 Replies

4,088 Views
igorpadykov
NXP Employee
NXP Employee

Hi Enrico

for i.MX8M mipi virtual channel is not supported in hardware, so the driver will not automatically

split the video from each virtual channel. The software can just receive the combined stream

into memory, then it needs split it if needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,088 Views
weichushun
Contributor I

Hi igor

The software can just receive the combined stream into memory, then it needs split it if needed.

---》are you sure that software can split the combined stream into 4 channels?  I am going to connect 8 cameras through the two MIPI CSI2

this is important, but I can not verify it in advance, thank you!

0 Kudos
Reply

4,088 Views
avismn
Contributor I

Hi Igor,

In case we are going to use two virtual channel. does the driver transfers all the data (VC0 + VC1) or does it ignore VC1 to VC3 ? 

Thanks,

Avi

0 Kudos
Reply

4,088 Views
igorpadykov
NXP Employee
NXP Employee

Hi Avi

driver receives all data, from all channels.

Best regards
igor

0 Kudos
Reply

4,088 Views
florian_hierl
Contributor III

Hi Igor,

is there already a software solution for separating the virtual channels in IMX8 ?

Has anyone tried this already ?

KR,

Florian

0 Kudos
Reply

4,088 Views
jude_federspiel
Contributor I

Hello Igor, your answer confirms what I've been reading. I want to input two cameras @720p/monochrome/30fps on two separate virtual channels into IMX8MMini, then encode H.264 on both separately. I gather from your post that I'll need to write code to manage the two virtual channels and the memory. Is there a simple way to estimate the processor loading for the memory management and encoding?

If you haven't sniffed it out, I'm an amateur. Mostly trying to evaluate a concept at this point.

Thanks in advance,

Jude

0 Kudos
Reply