iMX8M video support on weston

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M video support on weston

1,175 Views
sotero
Contributor III

Hello,

I'm trying to implement a video player on Weston using interface linux_dmabuf. The problem I see is that the pixel formats are not compatible with VPU decoder format (NV12). See available pixel formats in linux_dmabuf in Weston:

interface: 'zwp_linux_dmabuf_v1', version: 3, name: 11
        formats:
        'BA24'(0x34324142), modifier: 0x0000000000000000
        'RA24'(0x34324152), modifier: 0x0000000000000000
        'AB24'(0x34324241), modifier: 0x0000000000000000
        'AR24'(0x34325241), modifier: 0x0000000000000000
        'BA24'(0x34324142), modifier: 0x0000000000000000
        'RX24'(0x34325852), modifier: 0x0000000000000000
        'XB24'(0x34324258), modifier: 0x0000000000000000
        'XR24'(0x34325258), modifier: 0x0000000000000000
        'BG16'(0x36314742), modifier: 0x0000000000000000
        'RG16'(0x36314752), modifier: 0x0000000000000000
        'AB15'(0x35314241), modifier: 0x0000000000000000
        'AR15'(0x35315241), modifier: 0x0000000000000000
        'XB15'(0x35314258), modifier: 0x0000000000000000
        'XR15'(0x35315258), modifier: 0x0000000000000000
        'AB12'(0x32314241), modifier: 0x0000000000000000
        'AR12'(0x32315241), modifier: 0x0000000000000000
        'XB12'(0x32314258), modifier: 0x0000000000000000
        'XR12'(0x32315258), modifier: 0x0000000000000000
        'GR88'(0x38385247), modifier: 0x0000000000000000
        'R8  '(0x20203852), modifier: 0x0000000000000000

At the same time I'm seeing that gstreamer with waylandsink is unable to use accelerated video display due to the same reason: "waylandsink wlvideoformat.c:137:gst_video_format_to_wl_dmabuf_format: wayland dmabuf video format not found". The kmssink video sink works fine, but I need Wayland.

Am I doing something wrong? Is video supported in Weston?

Best regards,

Santiago Otero

0 Kudos
1 Reply

532 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Santiago,

Video processing is not supported by Weston in this moment you will have to wait until next release, or follow using kmssink.

Regards

0 Kudos