iMX8M plus based board resets abruptly after starting boot animation on Android 11 OS.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M plus based board resets abruptly after starting boot animation on Android 11 OS.

2,176件の閲覧回数
swapnilpendhare
Contributor III

We are starting with porting activity on iMX8MP based board with minimal hardware it includes 800x400 lvds display. We are using Android 11, which is part of requirement. 

We could enable only console interface and adb interfaces like USB/Ethernet is not yet configured and accessible. 

While booting system resets abruptly at around 60 seconds just after Android boot animation is initialized. 

As we have only one debug channel open i.e. serial console can anyone provide some suggestion on how to debug the reset problem 

To get more debug information, I have tried to execute logcat while boot is going on.
If we could just halt the system before reset and collect details about cause of reset would be very helpful.  

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,150件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Burn you image again for some reason the image is corrupted, so please try it again.

 

Regards

0 件の賞賛
返信

2,140件の閲覧回数
swapnilpendhare
Contributor III

We have tried to burn image multiple times and getting inconsistent results. 

We are utilizing uuu_imx_android_flash.sh script to flash the EMMC using serial download mechanism. 
We are not aware of any other/better mechanism to flash. 
Can you suggest improvement areas in this flash boot sequence. 

0 件の賞賛
返信