iMX8M: meaning of CSI2RX_BIT_ERR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M: meaning of CSI2RX_BIT_ERR?

651 Views
ensc
Contributor III

Hello,

reference manual says

pastedImage_1.png

Is the content of this register persistent?   E.g. assuming two transfers where the first one has a bad CRC and the second one is ok.  Will this register contain 7'b000_0000 (No error event) (from the 2nd xfer) or will it contain information about the error in the first transfer?

When content is persistent, how can I reset it?

When content is not persistent: how can I capture the information about bit errors?

0 Kudos
Reply
2 Replies

540 Views
jamesbone
NXP TechSupport
NXP TechSupport

Is the content of this register persistent? E.g. assuming two transfers where the first one has a bad CRC and the second one is ok. Will this register contain 7'b000_0000 (No error event) (from the 2nd xfer) or will it contain information about the error in the first transfer?

 ANSWER. Once some bit of this register is asserted, it will remain asserted until the register is read. When the register is read it's cleared.

When content is persistent, how can I reset it?

 ANSWER. Yes, it's persistent and is reset when the register is read.

When content is not persistent: how can I capture the information about bit errors?

 ANSWER. You can capture the information by pooling (reading periodicaly the register) or by interrupt using registers CSI2RX_IRQ_STATUS and CSI2RX_IRQ_MASK.

0 Kudos
Reply

540 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Enrico,

We are reviewing the RM internally so we can provide an accurate response.

0 Kudos
Reply