iMX8M is possible to use a Single SPI device on QSPI Interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M is possible to use a Single SPI device on QSPI Interface?

1,792件の閲覧回数
leandroschmitz
Contributor I

I need add 3x CAN bus and 4x 12 bits Analog Interface to my iMX8M Computer On Module.

To do these I need a extra SPI bus, I'd like to know if is possible to use the QSPI Interface .

Thanks

Regards

Leandro Schmitz

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,552件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Leandro

yes possible and for example it is described in

Figure 10-17. Serial Flash Access Scheme i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信