iMX8M eval board and AR8031 phy issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M eval board and AR8031 phy issue

782 Views
pnee
Contributor II

I'm using the i.MX8M evaluation target in JTAG boot mode.

But the AR8031 phy is unresponsive when I try to read some registers. I keep getting 0x0000 for all registers. I have tried all the possible PHY addresses and still I can't get anything other then 0x0000 from the registers. MDC is set to 2.5MHz.

Is there something specific that needs to be done to enable the PHY device?

0 Kudos
Reply
1 Reply

726 Views
igorpadykov
NXP Employee
NXP Employee

Hi PJ

may be useful to look at uboot codes enet initialization, in particular

function setup_fec() :

imx8mq_evk.c\imx8mq_evk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply