iMX8M Quad / iMX8M Plus Quad || PCIe Speed and Bandwidth

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Quad / iMX8M Plus Quad || PCIe Speed and Bandwidth

661 Views
JyotiVaishnav
Contributor II

Hello NXP Team, 

We are planning to use i.MX 8M Quad or i.MX 8M Plus Quad. 

Can you please share the details of the PCIe interface for both the processor how much Speed and Bandwidth both the processor will support.  . 

 

0 Kudos
Reply
3 Replies

644 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the i.MX8MQ has two pcie interface and the i.MX8MP has only one, for the pcie features you can see details in the RM, here take the i.MX8MP as example:

b45499_0-1695195477400.png

 

0 Kudos
Reply

624 Views
JyotiVaishnav
Contributor II

Hello @Rita_Wang 

Thanks for sharing the information. 

In iMX8M Quad there are two PCIe interface available, on one PCIe we are planning to connect the SSD and on the other PCIe AI Chip

Is it okay to connect ? 

0 Kudos
Reply

592 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you can use.

0 Kudos
Reply