iMX8M Plus SDIO external pull-ups necessary or internal pull-ups are enough? (For WiFi/BTH module)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8M Plus SDIO external pull-ups necessary or internal pull-ups are enough? (For WiFi/BTH module)

跳至解决方案
2,442 次查看
Charlie_Owz
Contributor II

Hi!

I have some doubts about the real need of externall pull-ups for SDIO lines used for a WiFi Module (in our case JODY-W2 by Ublox).

Due to reviewing some EVKs, I have seen that external pull-ups are not used for the SDIO lines, and we wonder if just with the configuration of the pin, in the NXP Pinmux tool, as "internal pull-up enabled" it would work.

Charlie_Owz_0-1625035626835.png

Is that right? Would that be enough?

Or on the contrary, Is it necessary to add the pullup?

 

Many thanks in advance.

标签 (1)
0 项奖励
回复
1 解答
2,439 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Charlie_Owz,

Use internal pull up, please! which is enough.

don't need external pull-up resistors.

 

Have a good day!

B.R,

weidong

在原帖中查看解决方案

2 回复数
2,254 次查看
at-at-at-at-at
Contributor I

plz, place external pull up resistor for test. some case(ATWILC3000-MR110xA), internal resistor is not enough.

0 项奖励
回复
2,440 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Charlie_Owz,

Use internal pull up, please! which is enough.

don't need external pull-up resistors.

 

Have a good day!

B.R,

weidong