Hi. @Chavira ,
Thank you for your reply.
I tried the patch you gave me, but there was no change in my symptoms.
Upon reviewing the logs, I have found additional information and have some questions to ask.
Additional information:
There are differences in the logs below between high temperature and room temperature.
Normal temperature: (Normal temperature, normal operation.txt L2918)
[drm:drm_helper_probe_single_connector_modes] [CONNECTOR:40:HDMI-A-1] disconnected
High temperature log: (High temperature, error operation.txt L2868)
[drm:drm_helper_probe_single_connector_modes] [CONNECTOR:40:HDMI-A-1] status updated from unknown to connected
・HDMI interface is not used
・Hardware pattern: All HDMI signals are open
However, at the time of the error, the log outputs that the HDMI was found even though the HDMI monitor was not connected.
Question:
Given the above, is there a possibility that something like this event will occur?
Please let me know if there are any other points that I should investigate.
Thank you for your support.
Best regards,