我使用 iMX8M Plus , imx-yocto-L5.10.52_2.1.0 系统,需要支持 LVDS+HDMI 两个显示器,分辨率不同。
现在发现,系统支持扩展模式,不支持复制模式。
我们想要的效果是启动 Qt 应用后,两个屏幕显示完全一样的界面。
这个有没有什么办法。
-------------------------------
I use iMX8M Plus, imx-yocto-L5.10.52_2.1.0 system, need to support LVDS+HDMI two monitors ,with different resolutions.
Now it is found that the system supports extended mode and does not support clone mode.
The effect we want is that after launching the Qt application, the two screens display exactly the same interface.
Is there any way to do this.
解決済! 解決策の投稿を見る。
Sorry, we do not support it. You can consider use the Android BSP.