iMX8M Plus 双屏显示问题(dual display)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Plus 双屏显示问题(dual display)

Jump to solution
535 Views
lishaocheng
Contributor III

我使用 iMX8M Plus , imx-yocto-L5.10.52_2.1.0 系统,需要支持 LVDS+HDMI 两个显示器,分辨率不同。
现在发现,系统支持扩展模式,不支持复制模式。

我们想要的效果是启动 Qt 应用后,两个屏幕显示完全一样的界面。


这个有没有什么办法。

 

-------------------------------

 

I use iMX8M Plus, imx-yocto-L5.10.52_2.1.0 system, need to support LVDS+HDMI two monitors ,with different resolutions.
Now it is found that the system supports extended mode and does not support clone mode.

The effect we want is that after launching the Qt application, the two screens display exactly the same interface.


Is there any way to do this.

0 Kudos
1 Solution
511 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Sorry, we do not support it. You can consider use the Android BSP.

View solution in original post

0 Kudos
1 Reply
512 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Sorry, we do not support it. You can consider use the Android BSP.

0 Kudos