iMX8M PCIe dual lane

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M PCIe dual lane

924 Views
OdedAvraham
Senior Contributor II

Hi 

Can the two ports of the iMX8M SOC be connected as one PCIe interface with dual lane? 

Purpose is to connect an M.2 SSD device as one PCIe 2.0 x2 (dual lane)?

If so, do both PCIe ref clock need to be feed? 

Thanks 

Labels (1)
Tags (1)
0 Kudos
1 Reply

667 Views
Yuri
NXP Employee
NXP Employee

 

Hello,

 

  i.MX8M has two PCIe modules, each supporting single lane  (PCIe Gen 2).

No ability to configure PCIe system as one PCIe interface with dual lanes.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos