iMX8M NANO with SD card can't install Android 10 but can install Android 11 by uuu.exe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8M NANO with SD card can't install Android 10 but can install Android 11 by uuu.exe

336 次查看
steveyang2
Contributor I

Try to use uuu.exe build Android 10 in windows 10 but meet error.

Please help me confirm the root cause.

 

Android Q10.0.0_2.6.0

Command :  .\uuu_imx_android_flash.bat -f imx8mn -c -e -t sd

Error message : 1/1 [HID(W):LIBUSB_ERROR_TIMOUT ] SDPS: boot -f u-boot-imx8mn-evk-uuu.imx.link

 

Android 11.0.0_2.4.0

Command :  .\uuu_imx_android_flash.bat -f imx8mn -c -e -t sd

Build successfully

0 项奖励
1 回复

325 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @steveyang2 

I run the same command with prebuilt images - android-10.0.0_2.6.0_image_8mnevk. and it works without such error.

Please check if all necessary software images that you are going to build for these command are included and without broken ones.

 

Best regards

Harvey

 

0 项奖励