iMX8M NANO with SD card can't install Android 10 but can install Android 11 by uuu.exe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M NANO with SD card can't install Android 10 but can install Android 11 by uuu.exe

333 Views
steveyang2
Contributor I

Try to use uuu.exe build Android 10 in windows 10 but meet error.

Please help me confirm the root cause.

 

Android Q10.0.0_2.6.0

Command :  .\uuu_imx_android_flash.bat -f imx8mn -c -e -t sd

Error message : 1/1 [HID(W):LIBUSB_ERROR_TIMOUT ] SDPS: boot -f u-boot-imx8mn-evk-uuu.imx.link

 

Android 11.0.0_2.4.0

Command :  .\uuu_imx_android_flash.bat -f imx8mn -c -e -t sd

Build successfully

0 Kudos
1 Reply

322 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @steveyang2 

I run the same command with prebuilt images - android-10.0.0_2.6.0_image_8mnevk. and it works without such error.

Please check if all necessary software images that you are going to build for these command are included and without broken ones.

 

Best regards

Harvey

 

0 Kudos