iMX8M Mini Windows 10 IoT with ili9811c LCD panel display debugging assistance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Mini Windows 10 IoT with ili9811c LCD panel display debugging assistance

3,261 Views
jesselin0420
Contributor I

Hi Experts,

Currently, we have successfully integrated the i.MX8M Mini processor with the BSP downloaded from the NXP website (W21H2-1-4-0), following the guidelines specified in the "i.MX Windows 10 IoT User’s Guide" to incorporate our custom board. The good news is that we can boot to UEFI without any problems.

However, upon entering Windows IoT, we encounter a black screen. Allow me to provide more details on our configuration:

     *Customized board with ili9881c MIPI DSI panel.
     *We have added the necessary driver and configured the ili9881c settings in u-boot, which resulted in a visible splash screen.

To address this issue, we are seeking your valuable guidance on debugging steps. Specifically, we would appreciate your expertise in helping us identify the root cause of the black screen issue in Windows IoT.

To assist you better, we have attached the log file, which contains relevant information that may aid in the debugging process.

Thank you for your time and consideration. We look forward to hearing from you soon.

 

Best regards,

Jesse

0 Kudos
Reply
15 Replies

3,068 Views
Michal_Minarcik
NXP Employee
NXP Employee

Hi @jesselin0420,

Can you please provide the resolution and parameters of the LCD panel you are connecting?

Thank you,

Best regards,

Michal

0 Kudos
Reply

3,061 Views
jesselin0420
Contributor I

@Michal_Minarcik 

below parameters are defined in the panel driver. You can find them in the patch I provided.

 

#define   LCD_XSIZE_TFT   720
#define   LCD_YSIZE_TFT   1280
#define   PCLOCK          62000
#define   LCD_VBPD        20
#define   LCD_VFPD        10
#define   LCD_VSPW        10
#define   LCD_HBPD        30
#define   LCD_HFPD        10
#define   LCD_HSPW        20
0 Kudos
Reply

2,908 Views
Michal_Minarcik
NXP Employee
NXP Employee

Hi @jesselin0420,

for i.MX 8M Mini it also needs to be modified in UEFI.

Open file mu_platform_nxp\Silicon\ARM\NXP\iMX8Pkg\Library\iMX8LcdHwLib\iMX8LcdHwLib.c

Add definiton for your display. According to the parameters provided, it should be as follows:

/* 720x1280@60Hz */
const IMX_DISPLAY_TIMING PreferredTiming_720x1280_60 = {
.PixelClock = 62000000,
.HActive = 720, 
.HBlank = 60,
.VActive = 1280,
.VBlank = 40, 
.HSync = 20,
.VSync = 10, 
.HSyncOffset = 10,
.VSyncOffset = 10,
.HImageSize = 0,
.VImageSize = 0,
.HBorder = 0,
.VBorder = 0,
.EdidFlags = 0,
.Flags = 0,
.PixelRepetition = 0,
.Bpp = 24,
.PixelFormat = PIXEL_FORMAT_ARGB32,
};

In the function below, select the desired resolution from the definition added above.

EFI_STATUS
LcdDisplayDetect (
VOID
)

/* Search for ADV7535 */
status = Adv7535Discover();
if (status == EFI_SUCCESS) {
DEBUG((DEBUG_ERROR, "ADV7535 probe SUCCEDED. Mipi-dsi display interface selected.\n"));
converter = ADV7535;
displayInterface = imxMipiDsi;
LcdInitPreferredTiming (&PreferredTiming_720x1280_60, &PreferredTiming);
break;

In the same file, the function below is called to initialize the NXP test panel. I assume you don't need any initialization, so it will need to be commented out.

Function:
LcdSetMode (
IN UINT32 ModeNumber
)

Comment:
CHECK_STATUS_RETURN_ERR(Rm67191Init(), "RM67191 config");

Best regards,

Michal

 

0 Kudos
Reply

2,554 Views
Michal_Minarcik
NXP Employee
NXP Employee

Hi @jesselin0420,

Have you tried the procedure I mentioned? Can I help with anything else?

Best regards,

Michal

0 Kudos
Reply

2,549 Views
jesselin0420
Contributor I

We still can't solve this problem. We can see the logo in the bootloader but then it's a black screen.

0 Kudos
Reply

2,537 Views
Michal_Minarcik
NXP Employee
NXP Employee

Hi @jesselin0420,

could you please try release W21H2-1-4-1 and make the adjustments I mentioned. If it helps?

For the next time, please let me know, when you need help. I was waiting for your reply to this ticket.

Best regards,

Michal

 

 

0 Kudos
Reply

2,526 Views
jesselin0420
Contributor I

Hi Michal,

Thank you for your attention.

Due to resource issues, this project is currently on hold. I'll inform you as soon as it's back on track.

 

Jesse

0 Kudos
Reply

3,222 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @jesselin0420 

Please share your company name.

Thanks

Zhiming

0 Kudos
Reply

3,175 Views
jesselin0420
Contributor I

Hi @Zhiming_Liu ,

  So .. what is the next step?

0 Kudos
Reply

3,170 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @jesselin0420 

Can you please share your changes about display panel?

I am asking WOA team.

Best Regards

Zhiming

0 Kudos
Reply

3,084 Views
jesselin0420
Contributor I

@Zhiming_Liu 

Still no feedback?

0 Kudos
Reply

3,128 Views
jesselin0420
Contributor I

@Zhiming_Liu 

is there any update from WOA team.

0 Kudos
Reply

3,077 Views
joanxie
NXP TechSupport
NXP TechSupport

the IOT team is working on this, any update, will share with you

0 Kudos
Reply

3,163 Views
jesselin0420
Contributor I

Hi @Zhiming_Liu 

  please see attached files.

0 Kudos
Reply

3,213 Views
jesselin0420
Contributor I
0 Kudos
Reply