iMX8M Mini / IoT Core: power management support?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8M Mini / IoT Core: power management support?

跳至解决方案
3,014 次查看
gennady_kuznetsov
Contributor I

Greetings,

we're evaluating power management capabilities of NXP's Windows 10 IoT Core BSP for iMX8 Mini EVK (W1860_1_0_1_IMX-IOTCORE-B191011). Power management is claimed to be supported, but powercfg reports only 

administrator@minwinpc1 C:\Data\Users\administrator>powercfg /A

The following sleep states are available on this system:

Hibernate
Fast Startup

The following sleep states are not available on this system:
Standby (S1)
The system firmware does not support this standby state.
Standby (S2)
The system firmware does not support this standby state.
Standby (S3)
The system firmware does not support this standby state.
Standby (S0 Low Power Idle)
Hybrid Sleep
Standby (S3) is not available.

 

For Hibernate, we're unable to receive positive results on EVK so far

1. First attempt to enable hibernation fails:

administrator@minwinpc C:\Data>powercfg /H ON
Hibernation failed with the following error: There is not enough space on the disk.

The following items are preventing hibernation on this system.
        The system could not create the hibernation file.  The specific error code is 0xc000007f.

2. Increased the size of the MainOS partition to ~3GB.
   Hibernation was enabled and hibernation file was created successfully.

 

3. The attempt to hibertate the EVK fails:

administrator@minwinpc C:\Data>shutdown /h
System will hibernate in 0 seconds...
Hibernate failed, 0x00000002

Could someone please advise how/if Hibernate is supposed to work?

Is there any other power management functionality available or planned?

Thank you in advance. 

0 项奖励
回复
1 解答
2,210 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Gennady

supported functionalities are described in sect.3 

BSP Supported Features i.MX Win 10 IOT Release_Notes

seems power management is not yet supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,211 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Gennady

supported functionalities are described in sect.3 

BSP Supported Features i.MX Win 10 IOT Release_Notes

seems power management is not yet supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,210 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Gennady

that resource is outdated and not more supported

pastedImage_3.jpg

GitHub - ms-iot/imx-iotcore: Windows 10 IoT Core BSP for NXP i.MX Processors 

Please use latest official documentation on

Windows 10 IoT Core for i.MX Applications Processors | NXP 

Best regards
igor

0 项奖励
回复