iMX8M L5.15.71_2.2.0 BSP issue with nnstreamer 2.2.0-r0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M L5.15.71_2.2.0 BSP issue with nnstreamer 2.2.0-r0

310 Views
mdouglas
Contributor II

ERROR: nnstreamer-2.2.0-r0 do_prepare_recipe_sysroot: The file /usr/lib/libprotobuf.a is installed by both tensorflow-protobuf and protobuf, aborting
ERROR: Logfile of failure stored in: /home/gitlab-runner/builds/wmaywjJA/0/odin/davinci/odin-yocto/build-odin/tmp/work/armv8a-mx8m-poky-linux/nnstreamer/2.2.0-r0/temp/log.do_prepare_recipe_sysroot.9351
ERROR: Task (/home/gitlab-runner/builds/wmaywjJA/0/odin/davinci/odin-yocto/sources/meta-psc/meta-ml/recipes-nnstreamer/nnstreamer/nnstreamer_2.2.0.bb:do_prepare_recipe_sysroot) failed with exit code '1'

This is the error I am getting in doing a yocto build.

0 Kudos
1 Reply

296 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The error indicates that you need a packages in your yocto system nnstreamer or you need to build the eIQ packages to add it to gstreamer and neural networks.

regards

 

0 Kudos