iMX8 max resulution for two display outputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 max resulution for two display outputs

1,015件の閲覧回数
greg_SOE
Contributor I

Hi,

I'm trying to understand the display capabilities of the i.MX8QM family. In the reference manual under the Display Controller Subsystem (page 5122), states that each Display Controller supports, among other features, "Two LVDS interfaces supporting...4k30 when aggregating the two interfaces".

For 4k30, which "the two interfaces" are being referred to? Does it refer to the two Display Controller interfaces, or the two LVDS interfaces per Display Controller?

Basically, is it possible to output a 4K30 signal from each Display Controller, whether it be through LVDS or DSI, or are both Display Controllers needed to produce one 4K30 output? Many SOM vendors don't mention anywhere near this capability, ususally topping out at 1080p per display.

 

Thanks,

-Greg

greg_SOE_0-1673986470418.png

 

0 件の賞賛
返信
2 返答(返信)

999件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There are two LVDS interfaces per Display Controller.and the MX8QM itself is 4K @ 30 fps, this can vary for you RAM, but thats for the chip.

regards

0 件の賞賛
返信

992件の閲覧回数
greg_SOE
Contributor I

It looks like the HDMI output supports 4k60 with 16bpp, so it sounds like the internal memory architecture can handle that kind of memory throughput.

 

What I'm interested in is if each DSI or pair of LVDS interfaces per Display Controller can individually output a 4K30 signal, for a total of two individual 4K30 outputs?

0 件の賞賛
返信