iMX8 flashing over USB stick

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 flashing over USB stick

2,102 Views
letan
Contributor III

I am working on the automotive project that is trying to use Android as OS. Currently we are targeting to support the flashing over USB stick.

So does Android or NXP support to flash over USB stick? If yes, then how?

Thanks,

Tan

0 Kudos
Reply
3 Replies

1,992 Views
b36401
NXP Employee
NXP Employee

Android supports such option.
However you need to make sure that the port you attach USB stick is USB master (or OTG) not slave.

1,992 Views
letan
Contributor III

Can you please point me where is such document of Android?

Thanks,

Tan

0 Kudos
Reply

1,992 Views
b36401
NXP Employee
NXP Employee

There is nothing special to i.MX.
When you attach USB stick to OTG port of the board it will be auto-mounted.

0 Kudos
Reply