iMX8 flashing over USB stick

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8 flashing over USB stick

2,109 次查看
letan
Contributor III

I am working on the automotive project that is trying to use Android as OS. Currently we are targeting to support the flashing over USB stick.

So does Android or NXP support to flash over USB stick? If yes, then how?

Thanks,

Tan

0 项奖励
回复
3 回复数

1,999 次查看
b36401
NXP Employee
NXP Employee

Android supports such option.
However you need to make sure that the port you attach USB stick is USB master (or OTG) not slave.

1,999 次查看
letan
Contributor III

Can you please point me where is such document of Android?

Thanks,

Tan

0 项奖励
回复

1,999 次查看
b36401
NXP Employee
NXP Employee

There is nothing special to i.MX.
When you attach USB stick to OTG port of the board it will be auto-mounted.

0 项奖励
回复