iMX8 flashing over USB stick

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 flashing over USB stick

2,118件の閲覧回数
letan
Contributor III

I am working on the automotive project that is trying to use Android as OS. Currently we are targeting to support the flashing over USB stick.

So does Android or NXP support to flash over USB stick? If yes, then how?

Thanks,

Tan

0 件の賞賛
返信
3 返答(返信)

2,008件の閲覧回数
b36401
NXP Employee
NXP Employee

Android supports such option.
However you need to make sure that the port you attach USB stick is USB master (or OTG) not slave.

2,008件の閲覧回数
letan
Contributor III

Can you please point me where is such document of Android?

Thanks,

Tan

0 件の賞賛
返信

2,008件の閲覧回数
b36401
NXP Employee
NXP Employee

There is nothing special to i.MX.
When you attach USB stick to OTG port of the board it will be auto-mounted.

0 件の賞賛
返信