iMX7ulp EVK board Debian (or some another user friendly) distro installing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7ulp EVK board Debian (or some another user friendly) distro installing

793 Views
ATAineri
Contributor III

Now I'm using the iMX6ul evk board and I have a lot of problems with yocto image. I need more userfriendly distro for working and I'm going to start using iMX7ulp (starting from EVK board).

There is very important if I can use some userfriendly distro on it and if it really possible how can I do this? Nevermind what he distro, but I prefer Debian 10. It may be Debian, Ubuntu, Fedora, CentOS in the end...

Labels (3)
0 Kudos
Reply
1 Reply

684 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vladislav,

Please take in mind that this images are not supported by NXP:

Debian on the i.MX6 sabre sd platform in a few commands 

https://community.nxp.com/docs/DOC-330147 

Regards

0 Kudos
Reply