HI ALL,
I'm using iMX7ULP to check how it works with eMMC.
While I tried pulling up the PIEZO_PWM pin which renders DDR mode for boot-up, it failed booting.
After getting failed, it just kept hanging in there. I couldn't fix it up through POR but Pin reset by toggling RESET 0/1.
I'm wondering why's that... cuz I found out from the datasheet as follows.
If it worked fine as mentioned above that POR would reset boot pins, it shouldn't've got this situation I suppose....
So could anyone tell me what's the difference between POR, PIN reset, RESET0/1?
Thanks.
Xinsun
RESET0 is the Power-On Reset (POR) signal for the whole SoC, whereas RESET1 only resets the A7 core.
Best Regards,
Artur
Hi @XinsunCHEN
So we understood from your statement that, After toggling the reset pin you are able to Boot.
This seems Power-up sequence-related issue.
Please confirm the reset pin is for i.MX7 not for other interfaces or power.
Regards,
Mrudang