iMX7ULP M4 clock configuration with SDK functions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX7ULP M4 clock configuration with SDK functions

881 次查看
markus4work
Contributor I

In my project, I start with the clock configuration the Boot ROM provides:

MCU running on FIRC @48MHz, DIV1-Platform and DIV2-BUS also @48MHz.

Now I want to configure e.g. the SIRC oscillator, Boot ROM configuration is SIRC on, but DIV1-Platform and DIV2-Bus deactivated.

I create the struct :

scg_sirc_config_t g_scgSircConfig = {.enableMode = kSCG_SircEnable | kSCG_SircEnableInLowPower,
.div1 = kSCG_AsyncClkDivBy1,
.div2 = kSCG_AsyncClkDivBy1,
.div3 = kSCG_AsyncClkDisable,
.range = kSCG_SircRangeHigh};
 
and call
CLOCK_InitSirc(&g_scgSircConfig);
to reconfigure the SIRC oscillator.
As probed with my Segger J-Link, the div1 value and the div2 value in register
SCG->SIRCDIV is not changed.
Checking the frequency with
CLOCK_GetFreq(kCLOCK_ScgSircAsyncDiv1Clk));
CLOCK_GetFreq(kCLOCK_ScgSircAsyncDiv2Clk));
gives the same result, Div1/Div2 still off.
When I call
CLOCK_SetSircAsyncClkDiv(kSCG_AsyncDiv1Clk, kSCG_AsyncClkDivBy2);
CLOCK_SetSircAsyncClkDiv(kSCG_AsyncDiv2Clk, kSCG_AsyncClkDivBy2);
afterwards, Div1/Div2 is set as expected to the chosen divider.
I monitor the same behavior for SOSC.
I need to provide a struct with the full desired configuration to
CLOCK_InitSirc(&g_scgSircConfig);
but the configuration is only set partially.
I now want to know if this behavior is intentional or a bug ?
 
Best regards,
Markus.
0 项奖励
回复
1 回复

858 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @markus4work,

I hope you are doing well.
 
Please mention where you are making a call to CLOCK_InitSirc().
 
- CLOCK_SetSircAsyncClkDiv is defined as below in SDK.
 
static inline void CLOCK_SetSircAsyncClkDiv(scg_async_clk_t asyncClk, scg_async_clk_div_t divider)
{
    uint32_t reg = SCG->SIRCDIV;

    switch (asyncClk)
    {
        case kSCG_AsyncDiv3Clk:
            reg = (reg & ~SCG_SIRCDIV_SIRCDIV3_MASK) | SCG_SIRCDIV_SIRCDIV3(divider);
            break;
        case kSCG_AsyncDiv2Clk:
            reg = (reg & ~SCG_SIRCDIV_SIRCDIV2_MASK) | SCG_SIRCDIV_SIRCDIV2(divider);
            break;
        default:
            reg = (reg & ~SCG_SIRCDIV_SIRCDIV1_MASK) | SCG_SIRCDIV_SIRCDIV1(divider);
            break;
    }

    SCG->SIRCDIV = reg;
}
 
- SIRCDIV is configured in CLOCK_InitSirc as below:
 
SCG->SIRCDIV =
        SCG_SIRCDIV_SIRCDIV1(config->div1) | SCG_SIRCDIV_SIRCDIV2(config->div2) | SCG_SIRCDIV_SIRCDIV3(config->div3);
 
So I don't think CLOCK_InitSirc implementation could be the issue.
 
 
Thanks & Regards,
Dhruvit Vasavada.
标记 (1)
0 项奖励
回复