iMX7Solo USB serial downloader not recognized

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX7Solo USB serial downloader not recognized

跳至解决方案
2,000 次查看
igal_kagan
Contributor I

Hello.

I'm using iMX7Solo device in my board. I'm trying to connect to the device by USB serial downloader, but PC not recognize any USB device. 

Note: I set BOOT_MODE to "01" and all the voltages are OK, RESET de-asserted. 

Screenshot 2021-01-14 193737.png

When I'm connecting with JTAG, it recognizes the Cortex A, and Cortex M cores without any problem. But no USB activity at all.

Please, help me to solve this issue.

Thanks.

Best regards,

Igor.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,952 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

My first suggestion would be to check that the VBUS supply on the OTG connector is default as off when the boards power up, and should be the processor which turn it on as specified n the Hardware design guide.

Does one of the snapshots correspond to this?

Best regards,
Aldo.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,984 次查看
igal_kagan
Contributor I

Additionals:

Power rails snapshot OK:

reset1.jpg

BOOT_MODE[1:0] pins are settled before RST de-asserted:

usb.jpg

eFuse Manufacturing mode is 1: 0x30350490=0x00800000

But, still there no USB detection on the PC...

Please, help me solve this issue.

 

Thanks.

Best regards,

Igor.

0 项奖励
回复
1,953 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

My first suggestion would be to check that the VBUS supply on the OTG connector is default as off when the boards power up, and should be the processor which turn it on as specified n the Hardware design guide.

Does one of the snapshots correspond to this?

Best regards,
Aldo.

0 项奖励
回复
1,948 次查看
igal_kagan
Contributor I

The problem was Vbus voltage.

Thanks a lot!

 

Igor.

0 项奖励
回复