iMX7S GPIO's in reset state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7S GPIO's in reset state

Jump to solution
651 Views
rfet
Contributor I

When we put the iMX7S in reset state (via POR-Input) after it was working, the GPIO's are still driven like they were before. Could you confirm, that the processor is not resetting his GPIO's while a POR-reset, in case it was running before?

Labels (1)
0 Kudos
1 Solution
561 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raphael

yes your understanding is correct as reset sequence starts after por release.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
562 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raphael

yes your understanding is correct as reset sequence starts after por release.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos