iMX7D custom board OV5640 not working in Android Marshmallow

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX7D custom board OV5640 not working in Android Marshmallow

1,537 次查看
shravan201
Contributor I

Hi All,

Please help to solve the problem. my project is delayed because of camera.

I am using iMX7D custom board with NXP Android M6.0.1_2.1.0 BSP (4.1 kernel).

problem : ov5640 is not working

camera driver probed properly and /dev/video0 node also created ...

Android camera open failed logcat :

*********************************************************************************

 959 I ActivityManager: Start proc 1370:com.android.camera/u0a33 for activity com.android.camera/.Camera
1370 I art     : Late-enabling JIT
1370 I art     : JIT created with code_cache_capacity=2MB compile_threshold=1000
 675 W art     : Long monitor contention event with owner method=void com.android.server.wm.WindowAnimator$1.doFrame(long) from WindowAnimator.
 1385 V CameraHolder: open camera 0
  834 I CameraService: CameraService::connect call (PID 1370 "com.android.camera", camera ID 0) for HAL version default and Camera API version 1
  834 W AudioFlinger: acquireAudioSessionId() unknown client 1370 for session 26
 1387 D NuPlayerDriver: notifyListener_l(0xb5f57680), (1, 0, 0)
  834 W AudioFlinger: acquireAudioSessionId() unknown client 1370 for session 27
 1389 D NuPlayerDriver: notifyListener_l(0xb5f57620), (1, 0, 0)
  834 W AudioFlinger: acquireAudioSessionId() unknown client 1370 for session 28
 1391 D NuPlayerDriver: notifyListener_l(0xb5f57320), (1, 0, 0)
  834 I CameraClient: Opening camera 0
  834 I FslCameraHAL: camera_device open: 0
  834 I FslCameraHAL: initialize name:csi, path:/dev/video0
  834 I FslCameraHAL: DeviceAdapter: Create ov5640 device
  834 I FslCameraHAL: sfmt[0]=NV12, dfmt[0]=YUYV
  834 I FslCameraHAL: sfmt[1]=YUYV, dfmt[0]=YUYV
  834 I FslCameraHAL: pixel format: 0x14
  834 I FslCameraHAL: sfmt[0]=NV12, dfmt[0]=YUYV
  834 I FslCameraHAL: sfmt[1]=YUYV, dfmt[0]=YUYV
  834 I FslCameraHAL: pixel format: 0x14
  834 I FslCameraHAL: SupportedPictureSizes is
  834 I FslCameraHAL: SupportedPreviewSizes is
  834 I FslCameraHAL: SupportedFPS is 15,30
  834 I FslCameraHAL: Preview callback not enabled c0d
  834 I FslCameraHAL: enableMsgType 0xc0d
 1395 D Camera  : app passed NULL surface
--------- beginning of crash
1395 E AndroidRuntime: FATAL EXCEPTION: Thread-116
1395 E AndroidRuntime: Process: com.android.camera, PID: 1370
1395 E AndroidRuntime: java.lang.NullPointerException: Attempt to invoke interface method 'java.util.Iterator java.lang.Iterable.iterator()' on
 a null object reference
1395 E AndroidRuntime:        at com.android.camera.CameraSettings.setCameraPictureSize(CameraSettings.java:126)
1395 E AndroidRuntime:        at com.android.camera.Camera.updateCameraParametersPreference(Camera.java:1950)
1395 E AndroidRuntime:        at com.android.camera.Camera.setCameraParameters(Camera.java:2070)
1395 E AndroidRuntime:        at com.android.camera.Camera.startPreview(Camera.java:1858)
1395 E AndroidRuntime:        at com.android.camera.Camera.-wrap13(Camera.java)
1395 E AndroidRuntime:        at com.android.camera.Camera$4.run(Camera.java:1112)
1395 E AndroidRuntime:        at java.lang.Thread.run(Thread.java:818)
 959 W ActivityManager:   Force finishing activity com.android.camera/.Camera
 959 I WindowManager: Screenshot max retries 4 of Token{da433d ActivityRecord{b622c94 u0 com.android.camera/.Camera t114 f}} appWin=Window{6e5c
83 u0 Starting com.android.camera} drawState=4

*********************************************************************************

My kernel patch:

*********************************************************************************

&csi1 {
       csi-mux-mipi = <&gpr 0x14 4>;
       status = "okay";

       port {
               csi_ep: endpoint {
                       remote-endpoint = <&csi_mipi_ep>;
               };
       };
};

&mipi_csi {
       clock-frequency = <240000000>;
       status = "okay";
       port {
               mipi_sensor_ep: endpoint1 {
                       remote-endpoint = <&ov5640_mipi_ep>;
                       data-lanes = <2>;
                       csis-hs-settle = <13>;
                       csis-clk-settle = <2>;
                       csis-wclk;
               };

               csi_mipi_ep: endpoint2 {
                       remote-endpoint = <&csi_ep>;
               };

       };
};

&i2c4 {
       ov5640_mipi: ov5640_mipi@3c {
               compatible = "ovti,ov5640_mipi";
               pinctrl-names = "default";
               pinctrl-0 = <&pinctrl_ov5640>;
               reg = <0x3c>;
               clocks = <&clks IMX7D_CLK_DUMMY>;
               clock-names = "csi_mclk";
               csi_id = <0>;
               pwn-gpios = <&gpio4 19 GPIO_ACTIVE_HIGH>;
               rst-gpios = <&gpio4 18 GPIO_ACTIVE_HIGH>;
               AVDD-supply = <&vgen6_reg>;
               mclk = <24000000>;
               mclk_source = <0>;
               status = "okay";
               port {
                       ov5640_mipi_ep: endpoint {
                               remote-endpoint = <&mipi_sensor_ep>;
                       };
               };
};

***********************************************************************

Thanks,

Shravan.

标签 (5)
标记 (3)
0 项奖励
回复
1 回复

1,309 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shravan

unfortunately for i.MX7D this is not supported in bsp according to attached Release Notes

Table 2. Features

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复