iMX7D GPIO1_IO03 Alt4 configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX7D GPIO1_IO03 Alt4 configuration

1,073 次查看
oferausterlitz
Senior Contributor II

Hello,

There was an option to configure GPIO1_IO03 pad of the iMX7D SOC to output 32kHz clock on the first releases of the pin configuration Excel files. Alt4 was osc32k.32K_OUT

Do you know why this option was removed from the Reference Manual and Pin Configuration program?Is option is still valid and working well on the iMX7D SOC.

Can you please tell us how this clock is produced and what is the source of this clock?

From our tests this clock is not sourced by the 32kHz crystal on the board.

Thank you.

0 项奖励
回复
2 回复数

932 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Ofer Austerlitz ,

     You can get related information from Reference Manual on website, see below, please!

----------------------------

pastedImage_1.png

Have a nice day!

NXP TIC weidong sun

0 项奖励
回复

932 次查看
jimmychan
NXP TechSupport
NXP TechSupport

According to the RM, there is no ALT4 option for GPIO1_IO03. That means this option is not valid to use.

According to the Table 5-11, the OSC_32K can be selected as clock source of CCM_CLKO2.

0 项奖励
回复