iMX7D BOOT_MODE0/1 correct supply to connect to?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7D BOOT_MODE0/1 correct supply to connect to?

Jump to solution
1,444 Views
chris_f
Contributor V

The IMX7DSHDG check list for Boot Mode inputs (Table 4) says you can tie or pull BOOT_MODE0/1 to VDD_SNVS_IN but according to IMX7DCEC those pins are in power group NVCC_GPIO1.

Shouldn't they be tied/pulled to NVCC_GPIO1?

Labels (2)
1 Solution
1,294 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Chris_F,

Thank you for pointing this error out! Indeed, the BOOT_MODE0/1 pins are in power group NVCC_GPIO1, so they must be tied/pulled to NVCC_GPIO1.

For reference, you can see that this is the configuration used on the i.MX7D SABRE board.

I’ll escalate this error on the HW Design Guide so it gets addressed in a future release. My apologies for the inconvenience.

Regards,

View solution in original post

3 Replies
1,295 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Chris_F,

Thank you for pointing this error out! Indeed, the BOOT_MODE0/1 pins are in power group NVCC_GPIO1, so they must be tied/pulled to NVCC_GPIO1.

For reference, you can see that this is the configuration used on the i.MX7D SABRE board.

I’ll escalate this error on the HW Design Guide so it gets addressed in a future release. My apologies for the inconvenience.

Regards,

1,294 Views
chris_f
Contributor V

Hi Gusarambula,

Thanks for the confirmation. Only other thing that I found in the HDG was what I assume is a typo or different for the Solo version: Table 7. gives recommendations for decoupling PVCC_GPIO_1P8_CAP but that doesn't exist on the iMX7D. I assume it should be PVCC_GPIO_CAP.

Regards
Chris

0 Kudos
Reply
1,294 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Chris,

Yes, that's also a mistake that's prevalent even on the Reference Manuals, where the PVCC_GPIO_1P8_CAP signal is also mentioned. I'll also escalate this. Thanks for the feedback!

Regards,

0 Kudos
Reply