iMX7 : share NAND between M4 and A7 core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX7 : share NAND between M4 and A7 core

1,868件の閲覧回数
victorien_vedri
Contributor I

Hi,

For a project, I would like a specific operating with iMX7 :

- Run FREERTOS on Cortex M4

- Run Linux/Yocto on Cortex A7

- Continual, Cortex M4 save data on NAND flash

- The main part of the time, Cortex A7 is sleeping and few time it wake up to process data (from NAND flash)

- NAND flash is share between Cortex M4 et Cortex A7.

Is it possible to have this configuration ?

Is there some example ?

Best regards

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,676件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi victorien

yes such configuration is possible, NAND can be shared using DRC described in

sect.3.2 Resource Domain Controller (RDC) i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Unfortunately I am not aware of examples of this case.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,676件の閲覧回数
victorien_vedri
Contributor I

Thinks for this answer.

Is there an application note which explain how to use the heterogeneous architecture (cortex M4 and A7) configure the cross compilation software and the SDK ?

0 件の賞賛
返信

1,676件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信