iMX7 : share NAND between M4 and A7 core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 : share NAND between M4 and A7 core

1,871 Views
victorien_vedri
Contributor I

Hi,

For a project, I would like a specific operating with iMX7 :

- Run FREERTOS on Cortex M4

- Run Linux/Yocto on Cortex A7

- Continual, Cortex M4 save data on NAND flash

- The main part of the time, Cortex A7 is sleeping and few time it wake up to process data (from NAND flash)

- NAND flash is share between Cortex M4 et Cortex A7.

Is it possible to have this configuration ?

Is there some example ?

Best regards

Labels (2)
0 Kudos
Reply
3 Replies

1,679 Views
igorpadykov
NXP Employee
NXP Employee

Hi victorien

yes such configuration is possible, NAND can be shared using DRC described in

sect.3.2 Resource Domain Controller (RDC) i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Unfortunately I am not aware of examples of this case.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,679 Views
victorien_vedri
Contributor I

Thinks for this answer.

Is there an application note which explain how to use the heterogeneous architecture (cortex M4 and A7) configure the cross compilation software and the SDK ?

0 Kudos
Reply

1,679 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply