iMX7 rise/fall time with 3.3V operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 rise/fall time with 3.3V operation

1,602 Views
justin_hsieh
Contributor I

Dear Team,

Our plateform is iMX7 with etherent application.

The ethernet Interface is RGMII which operation with 3.3V.

We find a case that tell the RGMII rise/fall time spec. should change to 1ns when 3.3V operation.

https://community.nxp.com/t5/T-Series/T1040-rise-and-fall-times-for-3-3V/m-p/601192

Does iMX7 can follow the 1ns rise/fall time spec. when RGMII powered at 3.3V?

 

Please advise,

Tks,

0 Kudos
Reply
5 Replies

1,596 Views
igorpadykov
NXP Employee
NXP Employee

Hi justin_hsieh

 

>Does iMX7 can follow the 1ns rise/fall time spec. when RGMII powered at 3.3V?

 

yes, as described in sect.4.10.3.3 Signal switching specifications 

i.MX 7Dual Family of Applications Processors Datasheet 

 

Best regards
igor

 

0 Kudos
Reply

1,587 Views
justin_hsieh
Contributor I

Hi Igor,

Sorry, We can't find the rise/fall time for 3.3 operation in sect.4.10.3.3.

Follow the case https://community.nxp.com/t5/T-Series/T1040-rise-and-fall-times-for-3-3V/m-p/601192

There is a formula for max rise/fall time calculate with different voltage operation.

The max rise/fall time t = LVDD[V]*(0.8-0.2)/2[V/ns].

For LVDD=3.3V this expression gives 0.99 ns.

So, the iMX7's rise/fall time spec. will be 0.99ns for 3.3V bank voltage.

 

Please advise,

0 Kudos
Reply

1,572 Views
igorpadykov
NXP Employee
NXP Employee

 

 

1.jpg

 

Best regards
igor

0 Kudos
Reply

1,560 Views
justin_hsieh
Contributor I

Hi Igor,

We had mesure the RGMII_TXC (pin ENET1_TXC)  rise/fall time at CPU side.

The results is  can't meet the 0.75ns when RGMII powered at 3.3V.

Please help dobule confirm the rise/fail spec. 0.75ns is suitable for 3.3V operation.

TX_CLK.jpg

0 Kudos
Reply

1,554 Views
igorpadykov
NXP Employee
NXP Employee

Hi justin_hsieh


>Please help dobule confirm the rise/fail spec. 0.75ns is suitable for 3.3V operation.


yes, datasheet valid for 3.3V operation too. Your issues may be related to board

layout, one can recheck it using sect.3.6.5. Impedance signal recommendations

Hardware Development Guide for i.MX7Dual and 7Solo Applications Processors

https://www.nxp.com/webapp/Download?colCode=IMX7DSHDG

also one can adjust drive strength DSE field in register IOMUXC_SW_PAD_CTL_PAD_ENET1_TX_CLK


Best regards
igor

0 Kudos
Reply