iMX7 VDD_ARM and VDD_SOC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 VDD_ARM and VDD_SOC

1,154 Views
lubomirfenic
Contributor I

Hi 

in the datasheet of iMX6 is written: VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source.

in the datasheet iMX7 is missing this kind of iformation.

Is it possible to supply both rails (VDD_ARM and VDD_SOC) from the same source?

Regards

Lubomir

Labels (1)
0 Kudos
3 Replies

738 Views
lubomirfenic
Contributor I

Hi Yuri,

thanks for answer.

If the voltage VDD_ARM is set to 1.1V then iMX7 can operate with max frequency 1GHz.

1.1V is still in recommended range for VDD_SOC.

I think that typ 1.1V is ok for VDD_SOC rail.

What is your opinion?

Regards

Lubomir

0 Kudos

738 Views
Yuri
NXP Employee
NXP Employee

Hello,

> 1.1V is still in recommended range for VDD_SOC.

> I think that typ 1.1V is ok for VDD_SOC rail.

Correct.

Regards,

Yuri.

0 Kudos

738 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Generally - yes, both suppliers may be provided from the same source,

but please pay attention on operating range specs in Table 9 of i.MX7 Datasheet(s).

Allowed voltage ranges for different modes are not the same for VDD_ARM_IN and VDD_SOC_IN.
The same source may be applied for run mode at 800 MHz and  below.

 

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf?pspll=1 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos