Hi,
We're using SOM which is based on iMX7 Dual for our project.
In which when the input source is removed which enters SNVS(+RTC) mode and the source is back which requires a low signal(using manual Switch) on MX7ONOFF which will transit SoC from SNVS to Normal mode.
Is there a way where we can avoid manual switch and as a power source is back it should boot without pressing a manual switch?
One option would be cut off SNVS supply and only run RTC when in no input source(this is aper their document).
But It'd be better with SNVS+RTC and boot without pressing a power(MX7ONOFF) button.
Application Note: Boot i.MX7 without pressing the power button
Thanks.