iMX7 Direct Boot from USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX7 Direct Boot from USB

2,211 次查看
Duracell
Contributor II

Hi

I currently have our iMX7 board booting from either SD card or EMMC. The option is configured using the GPIO pins.

I would like to be able to boot from USB using a USB flash disk or USB to SATA enclosure with an SSD drive. Is it possible to configure the boot GPIO pins to allow direct boot from USB or do I have to have uBoot on the either SD card / EMMC to boot linux from USB drive?

Thanks in advance

0 项奖励
回复
3 回复数

2,194 次查看
Duracell
Contributor II

Hi

I read the manual as sent prior to sending the question. It included USB boot options listed as follows:

"- USB (recovery mode) and plug detect (USB host stack not required in ROM, can bestored in an external boot device, e.g. serial flash)

- USB Solid-State Drive (via plug-in mode)"

I understood this as being able to boot from USB flash disk but per your response, it is not the case. Can you please help me understand what these two boot options actually mean?

 

Thanks in advance

 

0 项奖励
回复

2,191 次查看
igorpadykov
NXP Employee
NXP Employee

>Can you please help me understand what these two boot options actually mean?

 

please provide document where you find that.

 

Best regards
igor

0 项奖励
回复

2,202 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Duracell

 

unfortunately boot from USB using a USB flash disk is not supported.

So it is necessary to have uBoot. Supported  boot devices are described in

Boot Chapter of i.MX 7Dual Applications Processor Reference Manual

 

Best regards
igor